Part Number: TPS62060 Other Parts Discussed in Thread: TPS62811M Hi,
We have implemented TPS62060 device in our design. Vin=3.3V, Vout =1V
While Power ON we see an Inrush current of 2.6A for apprx.150uS. But our load current has to be apprx. 900mA…
Part Number: TPS62060 Hi team,
In an application that input voltage decreases slowly, I found the undervoltage lockout function kept getting triggered with the waveform shown as below
The purple line shows the output of TPS62060.
I think this…
Part Number: TPS62060 Dear Support,
Good day,
Kindly help to confirm only if the DC in the chip marking is matching the DC in the label for the part number TPS62060DSGR?
Please refer to attached photo for reference. Thanks
Part Number: TPS62060 Hi team,
Customer wants to comfirm the state of output impedance when the input voltage is zero. Is it Hi-Z?
They use this deivce at 5Vin, 3.3Vout. Then, they want to make the vout keep 3.3V at certain time after the input…
Part Number: TPS62060 Hi everybody!
I have a question about the "TPS62060" datasheet.
Q1) The absolute maximum rating of the SW terminal is described as -0.3 V to 7 V in the datasheet of this device. In the same document, the undershoot exceeds -1…
Part Number: TPS62060 Hi,
According to TPS62060 datasheet P. 11, "To minimize the current through the feedback divider network, R2 should be within the range of 120 kΩ to 360 kΩ. The sum of R1 and R2 should not exceed ~1 MΩ, to keep the network robust…
Part Number: TPS62060TPS62060,we use it to tranfer 3.3V input to 1.2V output, and it is supplied to DSP core, when the funcion mode of dsp is change suddenly, the output current ot TPS62060 changes from 0.7 to 1.1, and it causes 3.3V input unstable,…
Part Number: TPS62090-Q1 Other Parts Discussed in Thread: TPS62826 , TPS62823 , TPS62090 The datasheet for TPS62823 / TPS62826 mention following formula for inductor ripple current:
While the datasheet for TPS62090 mentions following formula:
…
Part Number: TPS62060 Other Parts Discussed in Thread: TPS62097 Hi all Would you minf if we ask TPS62060? <Question1> There is the description as follows on the datasheet P8; "During soft start, the switch current limit is reduced to 1/3 of its nominal…
Part Number: TPS62060 Other Parts Discussed in Thread: TPS62097 , TPS62085 I have a customer that would like to understand the transfer function of the internal compensation network for the TPS62060. What do we have that we can share with him?
Thanks…