Part Number: TPS62065 Hello
We find output of TPS62065 is not stable in our application. you can see the wave we test in file <Panel基板 Panel3.3V 電位異常検討_240305 2.xlsx>. We have something need you help to comfirm
1. We have taken many measures. If you…
Part Number: TPS62065 Tool/software: Hi Team,
The soft start time says 500us for the voltage to come up Below is the circuit sch snip attached, can you please confirm whether the delay provided to Enable pin can increase the delay from 500us to 1.5ms…
Part Number: TPS62065-Q1 Tool/software: Hi expert
Customer's PCB uses our TPS62065-Q1, currently customers need to work at ambient temperature 60℃, 90% ambient humidity, 1000 hours of continuous operation, Whether our chips can support it or not,…
Part Number: TPS62065 Tool/software: Dear team,
Can you please provide the footprint compatible part with larger start up time around 6ms from input to output.
Regards, Kaushal
Part Number: TPS62065-Q1 Tool/software: Hi team,
My customer have question about gain margin.
Here is customer phase margin test result. There are three 0 cross point in terms of phase.
Which cross point should customer refer?
Regards,
Youhei…
Part Number: TPS62065 Hi BU team,
I have some questions for you about the current limit of TPS62065:
When does the High Side tube turn on again after it is off due to current limiting? I noticed that the Ilimit of the upper and lower tubes is the…
Part Number: TPS62065 I'M so sorry to reply so late. we check the wave about SW, we found the wave of SW seems unnormal as below picture we force the mode pin to Vin and the IC should be work in PWM mode, but the the fsw change from 3M to 1.37MHz and…
Part Number: TPS62065-Q1 Hi, Support Team
Our client use TPS62065-Q1, Please help to review schematic as below chart
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: TPS62065-Q1
Hi, Support Team
We will use TPS62065-Q1, how to calculator ripple and Voutcap?
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence