Part Number: TPS62065 Other Parts Discussed in Thread: TPS62097 Hi,
we need to choose a 5V to 4.2V/2A DC/DC ,and require fast transient response, it is used as Power amplifier power supply.
could you give some suggestions. thanks.
Part Number: TPS62065 Other Parts Discussed in Thread: TLV62065 , Hi Team,
What is the difference between TPS62065 and TLV62065? I have compared these two sockets and haven't find more difference.
Thanks for your help!
Part Number: TPS62065-Q1 Dear team,
in the datasheet example, R1=360K, and the calculate Cff=17.6pF with the following formula, but finally we choose 22pf not 18pf. Could you please give me an explanation?
Thanks & Best Regards,
Sherry
Part Number: TPS62065 Other Parts Discussed in Thread: LMZ12003 We need to supply the decoupling network of an Spartan 6 Xilinx FPGA, the problem is that the required capacitance for this FPGA is around 600uF. We have being doing tests with an TPS62065…
Part Number: TPS62065-Q1 Hi,
My design information is below.
Device: TPS62065-Q1
Input voltage: 5V
Output voltage: 2V
Output current: about 500mA
Temperature: 25°C
Schematic as below attached.
When I measure the voltage of the FB pin, or lay a finger…
Part Number: TPS62065-Q1 Hi, Team,
Could you please give some information,
Does the device have Internal Pulldown resister on EN pin?
Thanks!
Best regards,
Koh
Part Number: TPS62065 Other Parts Discussed in Thread: LM26484 , , TINA-TI Tool/software: WEBENCH® Design Tools
Hi Team,
In my systems, there are many Ceramic capacitors at the DCDC output.
The capacitors are used to bypass different loades (FPGA etc…
Part Number: TPS62065 Hi team,
Recently my customer UAES has a question about the TJ, They want to know if there's some margin left for the maximum value of TJ(125℃).
Because they want to do a test under the condition of ambient temp=85℃. So they…
Part Number: TPS62065 Other Parts Discussed in Thread: TPS62095 , TPS62480 Dear, Sir.
ILIM range under Ta = -40 ~ +125 deng.C are defined on datasheet page 5,
min. 4.5A & max. 6.7A.
I wonder the value will be decreased when Ta going up?
Sorry to ask…