Part Number: TPS62065-Q1 Other Parts Discussed in Thread: TPS628502-Q1 Hi experts,
My customer seek SR which achieve 80%+ when current is 150uA. But in datasheet, efficiency only describe up to 1mA. Do you have 100uA~200uA efficiency data?
And do you…
Part Number: TPS62065-Q1 Hi team,
could you help on the following questions:
Time required for current/temperature detection,( this is the time from the temperature (current) anomaly to the shutdown of the output )
Whether the test is determined by multiple…
Part Number: TPS62065-Q1 Hi, Support Team
Our client use TPS62065-Q1, Please help to review schematic as below chart
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: TPS62065-Q1
Hi, Support Team
We will use TPS62065-Q1, how to calculator ripple and Voutcap?
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Part Number: TPS62065-Q1 We are using TPS62065QDSGRQ1 part in our design and whose output we are using to charge a supercapacitor. When there is no output from the regulator at the absence of input voltage to regulator and enable is below 0.4V, Supercap…
Part Number: TPS62065-Q1 Hi team,
Could you please help confirm maximum start up time of TPS62065-Q1? In datasheet the typical value is 500us and no min and max value.
Thanks,
Scarlett
Part Number: TPS62065-Q1 Hi TI expert
I looked the datasheet and it was unmarked ADAS information,please tell me whether TPS62065QDSGRQ1 can be used in ADAS application and ADAS products (QM/A/B/C/D) is QM?
Thanks
Jacob
Part Number: TPS62065-Q1 Hi team,
This is Jessica. glad to work with you.
i have a question about our TPS62065-Q1 design. As the datasheet described, the output L need to be 0.7uH to 1.6uH.
#1 if it possible for customer to use 2.2uH for their design(Vin…