Part Number: TPS62067-Q1 Hi Expert,
The car OEM is requesting how long this device's life span is. Do we have similar parameter like that? Or how long will this device's parameter not longer guaranteed? Or the expiration date? Thanks.
BR,
Elec …
Part Number: TPS62067-Q1 Dear team,
My customer use 62067-q1 with small output current. Vin=5V, Vout=3.3V, Iout=0.5A(max). Now I need to compute the inductor value, if the current ripple factor is 0.25, then the inductor should be 3uH based on datasheet…
Part Number: TPS62067-Q1 Hi
The datasheet says that TPS62067-Q1 devices has a built-in clock-dithering circuit. I am wondering what is the operation frequency of the build-in dithering circuit?
Thanks.
Part Number: TPS62067 Other Parts Discussed in Thread: TPS3702 , TPS386000 Dear Sir,
We are required to design the voltage monitor mechanism that meets below illustration. Currently, the PGOOD signal is used for power sequence and also false detect…
Part Number: TPS62067-Q1 Other Parts Discussed in Thread: TPS62065-Q1 Hi team
I would like to ask that when customer using TPS62067Q1 (2A max output) and customer actually outputs 0.3A, is that light-load condition?
Here is the customer schematic…
Part Number: TPS62067-Q1 Dear team,
Before I asked a question on E2E about the inrush current. We finally found that the inrush current comes from output capacitor. In our datasheet, we recommend 10uF~22uF. TPS62067-Q1 powers the MCU, and MCU requires…
Part Number: TPS62067-Q1 Hi,
do we have CTE info for TPS62067-Q1? It doesn't seem to be included in the "Quality, reliability and packaging data download" available on TI.com for this device.
Thanks!
-Sal
Part Number: TPS62067-Q1 Dear team,
My customer test IL( inductor current) of 62067, and they find there is a current pulse(max 2.4A) as below, but our device has no load when testing below waveform. Could you please help analyze why the inductor current…
Part Number: TPS62067 Dear TI Experts,
I use TPS62067 for 3.3V to 1.8V application~
And I bought 2kpcs TPS62067 last year,not from the agent.Everything is good~
And this year, I bought 1kpcs TPS62067,the output ripple is very big~
(The same PCB…