Part Number: TPS62067 Dear TI Experts
I have applied some TPS62067 for test but find below question(3.3V input,1.8V output, 300mA) really need your help:
I have welded three tps62067,only one can work well. the other two TPS62067 has ripples like…
Part Number: TPS62067-Q1 Other Parts Discussed in Thread: TPS62812-Q1 , Hi All,
As title, do you have SW pin min and max voltage limit on transient state?
like TPS62812-Q1 datasheet show [SW (transient for less than 10 ns)].
Thanks
BR,
…
Part Number: TPS62067-Q1 Dear Sir,
TPS62067-Q1 transitions between PWM and PFM mode automatically depending on the load condition.
What’s the threshold of the load condition for the transition? Like how many mA?
Or it happens on the DCM and CCM…
Part Number: TPS62067-Q1 Other Parts Discussed in Thread: TPS62090-Q1 , TPS62065-Q1
Dear *,
I have some questions regarding the stability of TPS62067-Q1:
First this is my configuration:
Iout is from 100mA to 350mA
1) What is the impact of…
Part Number: TPS62067-Q1 We are using this IC to generate 1.5V & 1.8V individually from 3.3.V.
Need the rise time & fall time of the internal FETs to calculate the switching loss.
Also, if there is short at the output side, will the IC retry after…
Part Number: TPS62067 Other Parts Discussed in Thread: TPS62065 , TPS62097 , TPS62822 Hi Team,
Can the PG pin of the TPS62067 be tied to ground? From my understanding tying an open drain output to ground should not damage the device.
My customer…
Part Number: TPS62067-Q1 Dear, Sir.
My customer is evaluation TPS62067-Q1. Now, they would like to estimate the
output accuracy on the product.
The datasheet defines the typical value of VFB(PFM) as 1%.
The other side, Figure 15 shows the accuracy…
Part Number: TPS62067-Q1 Dear, Sir.
My customer is considering to apply TPS62067-Q1 as the switching regulator for VIN=5V, VOUT=1.2V/2A.
The minimum on-time is not defined on the datasheet. So, I would like to make sure TPS62067-Q1 is no problem under…
Part Number: TPS62067 Other Parts Discussed in Thread: TPS62097 , TPS62822 , TPS62065 , Hi, team
Customer inquired how to reduce output ripple.
So, I asked to send operational waveforms at some key points.
The attached SW-pin waveform was sent for…