Other Parts Discussed in Thread: TPS62097 In theory, feedforward capacitor will introduce a zero and a pole, therefore can boost both the bandwidth and phase margin. However, in this paper, bandwidth narrows with increasing Cff, how to understand this…
Part Number: TPS62067-Q1 Other Parts Discussed in Thread: TPS62290-Q1 , TPS62260-Q1 Hi,
intention is to use TPS62067-Q1 in following constellation:
Vin = 5v0
Vout = 3v3
Iout = 0.49A
L = 1µH
Current ripple is approx. 70%.
Is it possible…
Other Parts Discussed in Thread: TPS62067 HI
I have downloaded te Spice model of TPS62067 and during simulation there is a 740mA current drawn at teh Avin pin when
TPS62067 EN pin is tie to Vin
TPS62067 EN pin is tie to ground
This should…
Other Parts Discussed in Thread: TPS62067 , TPS62065 , TPS62060 What is the load current level where the TPS62060 TPS62065; TPS62067 transitions into and out of PFM mode (power save mode)?
Other Parts Discussed in Thread: TPS62067TPS62067 Pre-Biase and soft start up Question.
TPS62067 Datasheet don't mention Pre-Biase function. Is TPS62067 Pre-Biase function?
Load sink case, TPS62067 soft start up without problem?
Regard.
Bob…
Part Number: TPS62065 Other Parts Discussed in Thread: TPS62067 , TLV62065 Hi Team,
Could you help to find the P2P solution of TPS62065DSGR?
We already find TPS62067, TLV62065.
Do we have more?
Thanks
Part Number: TPSM82822 Other Parts Discussed in Thread: TPS62067 Hi support team,
Is the pull-up resistor of the PG pin possible with 10kΩ? 100kΩ is used in the circuit example.
Regards, Dice-K
Also, it should be noted that Variant 006 (for Artix-7) and Variant 007 (for Spartan-7) use the same building blocks (TPS62067, TPS568215, and TPS65023B) to power the FPGA. Note that TPS62067 can be replaced by TPS62097, but TPS62097 was not released…
TPS65023-Q1 will also work, according to TIDA-01480. Keep in mind that you will need to find viable -Q1 substitutes for all single-rail regulators to create an Automotive non-safety power supply for XAZU5EV. The TPS568215, TPS56C215, and TPS62067 are…
Jon,
You will need at least version 15.7 or above since the model is encrypted. Alternately, try using the TINA-TI model for TPS62067. TINA-TI is a free simulator from TI.