Part Number: TPS62067-Q1 Hi,
do we have CTE info for TPS62067-Q1? It doesn't seem to be included in the "Quality, reliability and packaging data download" available on TI.com for this device.
Thanks!
-Sal
Part Number: TPS62067-Q1 Other Parts Discussed in Thread: TPS62067 Hi All,
In the datasheet of TPS62067, there is one sentence to define the feedback resistor value.
To minimize the current through the feedback divider network, R2 must be within…
Part Number: TPS62067-Q1 Other Parts Discussed in Thread: TPS62065-Q1 Hi team
I would like to ask that when customer using TPS62067Q1 (2A max output) and customer actually outputs 0.3A, is that light-load condition?
Here is the customer schematic…
Part Number: TPS62067-Q1 Dear team,
My customer test IL( inductor current) of 62067, and they find there is a current pulse(max 2.4A) as below, but our device has no load when testing below waveform. Could you please help analyze why the inductor current…
Hi Charlie,
It is not violating the limit. TPS62067-Q1 absolute voltage for the SW pin is DC ratings.
Please follow the app note: https://www.ti.com/lit/an/slva494a/slva494a.pdf?ts=1602503163849&ref_url=https%253A%252F%252Fwww.google.com%252F
Part Number: TPS62067-Q1 Dear Sir,
TPS62067-Q1 transitions between PWM and PFM mode automatically depending on the load condition.
What’s the threshold of the load condition for the transition? Like how many mA?
Or it happens on the DCM and CCM…
Part Number: TPS62067-Q1 Other Parts Discussed in Thread: TPS62090-Q1 , TPS62065-Q1
Dear *,
I have some questions regarding the stability of TPS62067-Q1:
First this is my configuration:
Iout is from 100mA to 350mA
1) What is the impact of…
Part Number: TPS62067-Q1 Dear, Sir.
My customer is evaluation TPS62067-Q1. Now, they would like to estimate the
output accuracy on the product.
The datasheet defines the typical value of VFB(PFM) as 1%.
The other side, Figure 15 shows the accuracy…
Part Number: TPS62067-Q1 We are using this IC to generate 1.5V & 1.8V individually from 3.3.V.
Need the rise time & fall time of the internal FETs to calculate the switching loss.
Also, if there is short at the output side, will the IC retry after…
Part Number: TPS62067-Q1 Dear, Sir.
My customer is considering to apply TPS62067-Q1 as the switching regulator for VIN=5V, VOUT=1.2V/2A.
The minimum on-time is not defined on the datasheet. So, I would like to make sure TPS62067-Q1 is no problem under…