Part Number: TPS61251 Other Parts Discussed in Thread: TPS62082 , , TPS61252 Hi TI Support team,
I have designed (PCB produced) a board that will be used to control some sensors (humidity, temperature etc). The board is also designed to drive two DC motors…
Hi ,Britta:
yes , I have already checked your suggestion , I think the load current is not exceed the maximum current ,because the load is an electronic device and it's very stable. So i will weld new board for test or I will try to test the TPS6…
Hi Aaron,
Thank you so much, TPS62082 (TPS62082DSG for 3.3V) look very promising.
Our current switcher, the LM3281, was optimized (according to the TI datasheet) for:
- powering noise sensitive wireless connectivity chipsets and RF Front end modules from…
Part Number: TPS62802 Other Parts Discussed in Thread: TPS62082 , TPS62088 , TPS62743 , TPS62748 The feature list on the TI website for both the TPS62802 and TPS62082 device lists "load disconnect". In the data sheets however, there is no mention of this…
Hi Aaron,
Thank you, I did saw that post before but I'm not sure what the part is for wireless application. Is TPS62082 a good choice for wireless application? Datasheet doesn't say. Does it have a lower noise compared to other DC-DCs?
Emilij…
Part Number: TLV62568 Other Parts Discussed in Thread: TPS62082 Hello,
I am planning to use the TLV62568 for stepping down voltage from 5V to 3.3V.
My load current fall under 500mA, which I feel would be the light load conditions for TLV62568 as its Iout…
This is explained in the 100% mode section (page 9). Efficiency generally doesn't change very much with small changes in Vin. It does change with the choice of inductor.
As well, this is an older device. Would the TPS62082 or TPS6209733 work for…
Part Number: TLV62084 Other Parts Discussed in Thread: TPS62097 , TPS62082 , TLV62568 Hi,
We are using TLV62084 for 5V -3.3V voltage regulation. Please find the portion of the schematic attached. In our proto boards, I observe that I am getting 3.24V only…
Part Number: LM3525 Other Parts Discussed in Thread: BQ24253 , TPS62082 , TPS61027 , TPS62081 , The system is meant to powered via a single cell 3V7 LiPo battery.
The board is using the BQ24253 as a battery charger / power path management.
This IC is working…
Other Parts Discussed in Thread: TPS62082 , TPS62080 Support,
We have a customer interested in the TPS62080. As a standard practice, the customer normally spreads some bulk caps through the board, about 100uF each. The TPS62082 has a note saying that it…