Part Number: TPS62085 Hi,
Kindly share the part number if there is an automotive-grade replacement for the TPS62085 with a pin-to-pin footprint compatibility.
Part Number: TPS62085 Other Parts Discussed in Thread: TPS7A8101 HI Team, I am using the TPS62085 and TPS7A8101 in my design I need Pspice simulation model is not avilable how can i get Pspice model.
Part Number: TPS62085 Tool/software: Hi team,
My question is whether the VOS Pin can be floated? The competitor is SGM61303, which is floated in this Pin and is the main AVL device in ctm side. If TPS62085's VOS pin can be floated, ctm can introduce…
Part Number: TPS62085 Other Parts Discussed in Thread: TPS62827 Hi Team,
just want to check if there is p2p device with TPS62085 but can support 4A . Thanks.
BRs
Given
Part Number: TPS82085 Other Parts Discussed in Thread: TPS62085 , Hello,
Does the TPS82085 use the same die as the TPS62085?
Best regards,
Denis GALLARDO
Part Number: TPS62085
Hi team,
I am having issues measuring over the switching frequency:
Their test results:
I can understand that under light load, the f sw is reduced to save power.
I have also read the following application note:
Understanding…
Part Number: TPS62085 Other Parts Discussed in Thread: TPS54625 , Dear Team,
The Pull-up of Reference PG is recommended to be 1Mohm, because the PG has EN pulled to two LDO & TPS54625, As a result, the PG of TPS62085 is only 1.43V, which cannot meet…
Part Number: TPS62085 Good morning,
I checked the switching node of the IC when the load is close to 0A, a little bit more than 1A and a little bit more than 3A.
With no load IC enters the PSM mode as expected.
With a 1A load, switching frequency…