Part Number: TPS62086 Other Parts Discussed in Thread: TPS628303 , TPS62865 Tool/software: You wrote on your site that you recommend the newer TPS62826DMQ instead of TPS62086. Can I learn the end of life status of TPS62086? You recommend it because it…
Part Number: TPS62086
Hello,
I have been designing with LTE/4G modules for many years and I use TPS62086 for power.(used in 20k+ pieces board) LTE module manufacturers recommend 2 parallel 470uF tantalum capacitors in the module power circuit(3.3V…
Part Number: TPS62086 In a project we have, we need 3.3V as output and the minimum input voltage that we have is 3.35V (from a Li-Ion cell output) and during this state we set our device into a deep sleep mode, getting a 120uA current consumption. The…
Part Number: TPS62086 Do I need to pull up the power good pin for the output discharge function to work on the TPS62086? I don't use the power good feature, I don't need this feature. Do I still need to pullup with a 1M resistor, as in the example schematic…
Part Number: TPS62086 Hi.
We are using the TPS62086 in a project we have where we need 3.3V as output. TPS62086 has as an input a 3.6V or 3.7V cell.
In rare cases when the cell is fully drained and it is charged to the minimum voltage to have 3.3V…
Other Parts Discussed in Thread: TPS62086 Hi,
i search for 3D file (STEP or IGS) for the TPS62086 package.
The package is VSON-HR 7pins 2x2mm
Thanks for your help.
Regards
Other Parts Discussed in Thread: BQ24392 , BQ24295 , BQ51013B , TPS62086 , BQ51050B Hi, I am building some modular boards for prototyping. I have designed a USB based solution for 3.3V using a BQ24392 negotiating high current for a TPS62086. Now I would…
Part Number: TPS543321 Other Parts Discussed in Thread: TPS62135 , TPS62086 , TPS62868 , TPS62869 , TPS62150A Hi team,
My customer has been looking for the dcdc converter which meets the requirements below. Could you please kindly confirm if we have…
Part Number: TPS62132 Other Parts Discussed in Thread: TPS62086 , TPS62903 , TPS61232 Hi,
I designed a step down converter for the 4G module. A regulator like the TPS62086 would have been easier, but I had to choose the TPS62132 because it was not in…