Part Number: TPS62090-Q1 Other Parts Discussed in Thread: TLV62569 , TPS62090 Hi,Sir:When designing the WIFI communication module, we used TLV62569PDDCR as the PA power supply (1.8V 500mA), but the performance was not satisfactory (the EVM index was poor…
Part Number: TPS62090-Q1 Tool/software: Can the PG pin drive a RESETn signal? or DO I need to add a buffer? Logic will be PG=High, resetn=High and when PG=low, RESETn=low.
Part Number: TPS62090-Q1
Tool/software:
Hi Team,
Could you please help to clarify what is the different between RJB and RJCbottom? Why RJCbottom is so low?
If we want to input the RJB into thermal simulation tools, which one should we refer? …
Part Number: TPS62090-Q1 Tool/software: Hi team,
My customer finds the PWM mode switching frequency of TPS62090-Q1 is 2MHz in their test, which should be 2.8MHz from the datasheet. The test condition are [Vin=3.3V, L=1uH, Vo=1.8V, Io=0.55A] and [ Vin…
Part Number: LM76005-Q1 Other Parts Discussed in Thread: TPS62090 , LM76005 Tool/software: Hi,
Please help review the power supply design for LM76005 and TPS62090. Thank you.
LM76005-TPS62090.pdf
Part Number: TPS62090-Q1 Hi team
I would like to get your confirm that are there any other differences between TPS62090QRGTRQ1 and TPS62090RGTR besides AECQ qualification/test?
Part Number: TPS62090-Q1 Other Parts Discussed in Thread: TPS62090 , Hi team,
I see the Tj is same between these two parts.
Could you please tell me why TPS62090 operation temp is up to 85 degreeC but TPS62090-q1 op temp is up to 125 degreeC…
Part Number: TPS62090-Q1 Hi Ti member,
About the switching note of SW output, whether have a spec to definition the overshoot & undershoot?
I know datasheet have SW(max) = Vin +0.3(V) / SW(min) = -0.3(V) in Absolute Ratings table. but it is correct…