Part Number: TPS62095 Hi team,
Just want to check with you about the SS pin voltage after powering up? According to the datasheet, the typical SS voltage is 1.25V.
However, according to the customer's test, the SS pin voltage is 5V. Customer test 5 pcs…
Part Number: TPS62095 Hi Team,
We would like to set “VOUT=0.8V= VREF”.
Then, we set those feedback Resistors R1=100kohm and R2=Open.
Is there any problem?
And, could you please let us know if you have any recommended value of R1?
Regards…
Part Number: TPS62095 Dear, Sir.
I think DEF pin is for internal logic supply, so must be connected to AVIN.
If the pin will be floating or connected to GND, the device could not work
because the internal logic was disabled.
I wonder above my understading…
Part Number: TPS62095 Other Parts Discussed in Thread: TPS62090 , Hello team,
Do you have any plan to release higher switching frequency version TPS62095? TPS62090 have 1.4MHz/2.8MHz version option.
Thanks.
Best regards,
Dongba o
Part Number: TLV62095 Other Parts Discussed in Thread: TPS62095 Hi ,
I used TPS62095 in my design. My manager asked the second source. Then i saw TLV62095 is pin-to-pin compatible to TPS62095 and even cheaper.
Can anyone told me the difference betwee…
Part Number: TPS62095 Hi team,
I have two questions about TPS62095:
If Vin=5V and Vout=1.2V/1A, what's the switching frequency? 1.4MHz or 1.2MHz? I can't see clearly from D/S, my customer's test result is 1.2MHz, could you help confirm?
How…
Other Parts Discussed in Thread: TPS54426 , TPS62095 I'm seeking feedback regarding the TPS62095 vs the TPS54426, both 4A buck regulators. I have used the TPS54426 before, and I was just testing it on the lab bench again. I get solid efficiency numbers…
Other Parts Discussed in Thread: TLV62095 , TPS62095 I've looked through the datasheets for the above two devices, and can't find anything notable enough to warrant separate part numbers or the cost difference. It's possible I've missed something…
Other Parts Discussed in Thread: TPS62095 Hi Everyone,
Please let me ask about enable control. I understand that the EN pin has 400kohm active pull down, then is TPS62095 disabled when EN pin is floated?
It's appreciated if you can tell the recommended…
Other Parts Discussed in Thread: TPS62095 I'm testing the possibility of using the TPS62095 at a lower voltage on the FB pin than the standard 0.8 V. I'm doing this by controlling the voltage on the SS pin, since the FB pin tracks the SS pin, divided…