Other Parts Discussed in Thread: TPS62120 , TPS62122 We're evaluating the TPS62120 buck converter. We'll ultimately fix the output voltage in our design, and I'm wondering if there's a fixed voltage output part (3.3V) I should look at.
Other Parts Discussed in Thread: TPS62120 , TPS62125 My piezoelectric vibration energy harvesting setup might require a bridge rectifier before input to TPS62120. Does T.I. have a product similar to LTC3588-1 that has a bridge rectifier integrated? If not…
Other Parts Discussed in Thread: TPS62120 Hello,
I'm developing a device which uses the TPS62120 to generate a -1.6V supply rail for operational amplifiers. The performance in terms of efficiency, noise, regulation and so on is entirely satisfactory,…
Part Number: TPS563210A Other Parts Discussed in Thread: TPS62120 Hi Team,
I encountered an error while importing the PSPICE model of TPS563210A. Unfortunately after going through the creating new Macro this error appeared "Undefined parameter or possible…
Other Parts Discussed in Thread: TPS62120 , TPS54040
I need to produce +5V @ 60mA and -5V @ 20 mA from 15V.
The loads are not symmetrical so direct split-rail generation with a coupled inductor ( http://www.ti.com/lit/htm/slva369 ) is not an option, or…
Other Parts Discussed in Thread: TPS62120 Hi All,
The TPS62120 Vout looks long time to turn on when EN already pull high.
We use TI EVM board to do the test and test condition:(Vin=12V, Vout=3.3V, Iout=0.06A) & We use electrical load, not R Load.…
Other Parts Discussed in Thread: TPS62120 , TPS54040 , TINA-TI
Hello.
I cannot simulate TPS62120 or the TPS54040 in my TINA spice simulator. I
believe that the problem is because the TI library I downloaded from
TI's web site is ENCRYPTED. I purchased…
Hello Matt,
Thanks for your reply,
I have now 2 more interrogations :
- What are the parametres for the circuit Fig 2 ( https://www.ti.com/lit/an/snva801/snva801.pdf?#page=3 in ordrer to implement it on LTSpice ?
- For the Equation 8 of the attached…