Tom,
It seems to me that we are getting hung up on the terminology here, and it is not the input impedance of the TPS62122 device that you need for your model. Instead, it sounds like you are trying to model the "effective load" that your Energy Harvesting…
Part Number: TPS62122 I have a 6.6 volt input for Vin and only 1 ma of current available limited by a constant current diode. My supply has 2 outputs 2.7 and 1.8 using 2 of the TPS6212s. I power up fine but if I raise the input power slowly or jiggle…
My schematic is the same as TIDA-00690 eval board.
If I supply separetely TPS62122, the efficiency is about 80-85% but the context is different : with a power supply the DCDC is in "constant mode". With the harvester, we consider the transient of start…
Part Number: TPS62122 I'm surveying Buck converter. The condition is as below:
Buck converter: input voltage >= 7V, output voltage: 2V ,Iout>0.05A, ultra low Iq, smaller package.
Is TPS62122 the best solution? Thanks.
Part Number: TPS62122
In the data sheet of TPS62122, there says Output Current is 75 mA.
I have two questions for this output current.
1. Is this mean TPS62122's maximum capable current is 75mA? What happens is loader takes more current than 75mA?…
Part Number: TPS62122 Hi, looking for every option to save power in battery designs I would like to save the diode that typically sits between the battery (coin cells or whatever small stuff) and the power circuit.
This diode takes ~ 0.5V of my small power…
Part Number: TPS62122 Other Parts Discussed in Thread: TPS61222 Hi,
Does TI have a power supply similar to TPS61222DCKT. The issue I am having with the TPS61222 is that the output voltage during shutdown is still present. I am looking for a power supply…
Part Number: TPS62122 Other Parts Discussed in Thread: TLV713P , This is related to our an earlier question we asked, link below please
We are designing a 12V to 3.3V (Buck + LDO) Power Supply for Bluetooth MESH network. We are using TPS62122 to step down…
Part Number: TPS62122 Other Parts Discussed in Thread: TLV713P , This is related to an earlier question we asked, link above
We are designing a 12V to 3.3V (Buck + LDO) Power Supply for Bluetooth MESH network. We are using TPS62122 to step down 12V to 3…