Other Parts Discussed in Thread: TPS62122 , CC1175 Hello, we have a new design with TPS62122 as DC/DC regulator for a TI CC12xx RF device. There is significant unwanted noise floor at TPS power output, that creates mirror peaks left and right of the RF output…
Other Parts Discussed in Thread: TPS62150 , TPS62122 Hi,
can you translate the models of the DC-DC-Converter TPS62122 and TPS62150 for use with Tina or LTSpice?
Regards
H. Schwär
Hi GGA,
If you can accept Vout follows VIN, not regulated, Yes, some bucks can support, like TPS62122.
As we can check that VIN UVLO of TPS62122 are VIH=0.8V, VIL=0.6V respectively. For these lower UVLO parts, the internal circuit design is much more…
Part Number: TPS62120 Other Parts Discussed in Thread: TPS62122 Hello experts,
Do you have EOL plan of TPS62120/TPS62122?
My customer wants to know EOL information.
Thanks and best regards,
Ryo Akashi
Other Parts Discussed in Thread: TPS62120 , TPS54040
I need to produce +5V @ 60mA and -5V @ 20 mA from 15V.
The loads are not symmetrical so direct split-rail generation with a coupled inductor ( http://www.ti.com/lit/htm/slva369 ) is not an option, or…
Koti,
I believe the problem you are seeing is caused by the additional loading of the output capacitance during start up which is causing the input capacitor to discharge below UVLO due to your current limited voltage supply.
I would not expect that simply…
Part Number: TPS62120 Other Parts Discussed in Thread: TPS62122 Hey TI
In the datasheet for TPS62120/2 under inductor selection it is recommended/warned that the design uses an inductor with a quality factor of less than 25. Then it proceeds to recommend…
Part Number: TIDA-00690 Other Parts Discussed in Thread: TPS62125 , TPS62122 I've got two questions regarding TIDA-00690
1- Can we buy it? If so, where.
2- Can it give 3V output power?
Part Number: BQ25504 Other Parts Discussed in Thread: TPS63030 , , TPS62122 Like the title alludes, I have two separate IC's, both TI parts as well and tied to the same voltage source, to get a 1.9 V rail and 3.0 V rail for the rest of my design. I know…