Part Number: TPS62125 Other Parts Discussed in Thread: TPS629210-Q1 , TPS629210 , TPS629206 , TPS629203 Hi
I am designing a power supply for Xbee3 module. Digi's documents recommend to keep switching above 500kHz if using a switcher. Xbee3 module draws 18mA…
Part Number: TPS62125 Other Parts Discussed in Thread: TPS62170 , TPS62160 Hi,
I use a TPS62125 in a design in inverting configuration for low consumption usage (4 mA max).
The inverted voltage have to be able to reach -9.4V with a Vin at 3.3V.
Our design…
Part Number: TPS62125 Hi,
I am using TPS62125DSGR in my design which has 12 V at input voltage and 'Sensor_en' as the enable signal coming from FPGA. The ideal output at the output of TPS62125DSGR should be 2.82V. This 2.82 V is given to a LDO …
Part Number: TPS62125 Other Parts Discussed in Thread: TPS62170 Hi Team,
My customer is currently looking for a drop-in replacement for our TPS62125DSGR to continue to support their supply chain since we have no available stock for this part. Do we have…
Part Number: TPS62125 We are currently using the TPS62125 in two very similar products. The layout and components associated with the TPS62125 sub-circuit are exactly the same, 6 volt input, 3.5 volt out. The loads are also very similar, both are under…
Part Number: TPS62125 We have an application to derive the power for the micro-controller (3.3V/10mA) from the 4-20 signal, we are considering TPS62125 for this application. Please let us know if this is the right part and share the application circuits…
Part Number: TPS62125 Hello,
We use the TPS62125 buck converter in a few designs, we are having some noise issues in one of the batch of the boards and wondering any suggestion to fix and any reason for the cause would be very much appreciated. All PCB…
Part Number: TPS62125 Hello community!
I am working on a project where i should build buck converter(from 12-14.4v to 2.85V/300mA) that connected to LED which consumes 2.85v with 300mA.
When i run DRC, I am having 4 of unconnected items issue mostly due…
Part Number: TPS62125 Other Parts Discussed in Thread: TINA-TI Hello all,
I simulated with TPS62125 to check the difference between input current with input cap and without input cap in the Tina-ti.
The below pictures are the file that I download in…
Part Number: TPS62125 Hi,
I'm trying to implement the TPS62125 Enable Threshold and Hysteresis settings (EN and EN_hys pins). The datasheet Application section is clear about how resistors R_EN1 and R_EN2 affect the enable thresholds. However, there's…