Part Number: TPS54678 Other Parts Discussed in Thread: TPS62130 , , TPS62824A , TPS62802 , TPS62A01 Dear TI team,
I am using tps54678 and tps62130 for my project. IC tps54678 has boot pin while tps62130 do not have boot.
What is the difference between…
Part Number: TPS62130 Tool/software: dears,
the customer wondering how tps62130 works when over current happens, in what condition, the over current will lead to TPS62130 to shutdown?
the datasheet just described how current limit works, but does…
Part Number: TPS62130 Tool/software: Hi there,
i have a problem with my circuit and the TPS62130RGTR.
Under slight load (10-50mA) the output is perfectly fine at around 3.2x volts.
But when i start to switch on the load (37 LEDs) the voltage drops…
Part Number: TPS62130 Tool/software: Hello Team,
Please help to review the schematic sections adhering to TPS62130RGTR controller from TI.
Power Architecture block diagram also included.
Please help and share your feedback.
4375.ti_power_review_20250310…
Part Number: TPS62130A Tool/software: Hi Teams,
When the switching frequency is 1.25MHz, VIN=5V, Vout=1V, Iout=1.29A, The conversion efficiency of TPS62130ARGT is only about 67%, which is significantly different from the theoretical conversion efficiency…
Part Number: TPS62130 Other Parts Discussed in Thread: TPS5430 Tool/software: Hello TI team,
I am designing a power supply that needs to step down from 19.5 V DC (input) to 5 V DC (output) with a maximum load current of 1.5 A.
Key requirements: -…
Part Number: TPS62130 Tool/software:
Hi TI experts,
The circuit design of TPS62130RGTR is shown in the figure below .
We conducted the electrical performance testing on the TPS62130RGTR according to its rated maximum current of 3A, although our…
Part Number: TPS62130 Tool/software: Hi,
Recently,
During Board Rework, We removed the Resistor to GND at FB pin of regulator and powered on the board, The regulator stops working, it outputs Constant Voltage,
Later we mounted the Resistor Back…
Part Number: TPS62130 Other Parts Discussed in Thread: TPS62933 Tool/software: Dear,
Could I use TPS62130 DCDC converter to get Vout = 9V, from Vin = 12V, estimated Iout should never exceed 1.5 A?
If yes, how to calculate R1 and R2, and some other…