Part Number: TPS62130A Other Parts Discussed in Thread: TPS62130 , Hi team,
My customer got a reel with TPS62130 AG RGTR partnumber.
They asking what letter AG means?
Looks like letter A mean that PG pin have power good l ow login level.
But I'm confused…
Part Number: TPS62130A Other Parts Discussed in Thread: TPS62135 What is the switching frequency range of the TPS62130A? I would like to check if there is no problem with the current circuit, which is up to 2.81 MHz.
Part Number: TPS62130A Other Parts Discussed in Thread: TPS62130 , What is the PG pin used for and what are the differences between the TPS62130 and TPS62130A?
Part Number: TPS62130A-Q1 Dear team,
This device is used to power the USB. When the customer hot plug the USB several times, our device has no output. At the same time, VIN and EN is normal. I am not sure whether our device is damaged. Could you please…
Part Number: TPS62130A We use TPS62130A on our custom board and now I am testing. Used of condition is below. Vin = +5V, Vout = 3.3V and +2.5V (Number of TPS62130A on the board is two.) We measured voltage of Vout and Vin with oscilloscope in the power…
Part Number: TPS62130A Hi Sirs,
The TPS62130A design spec is
Vin: 3.3V;
Vout: 1.15V
I_load: 0.16A
Fsw: 1.25MHz
Could you help check the switch node at light loads (0.16A), is it operating in power save mode?
We measure the min switching level is -0…
Part Number: TPS62130A Dear E2E Design Support,
I have been using the TPS62130A in several designs, but recently I encountered a radiated emission issue with a new board which made me thinking about the right layout topology, especially how to connec…
Part Number: TPS62130A Is there any significant leakage into the TPS62130A when VIn is powered down (0V) and voltage (say 3.3V) is applied to the PG pin?