Part Number: TPS62133 Tool/software: On the +5V-Output of the TPS62133 power supply is a raspberry 3B+ connected. In some cases the raspberry can parallel powered over usb-c connector with an external 5.2V/2.4A power supply. The external 5.2V power supply…
Part Number: TPS62133 Other Parts Discussed in Thread: TPS62130 , Hi
I am using TPS62130 to generate a 5V voltage in a mass production product. I want to know is there any risk if I directly replace TPS62130 with TPS62133, don't remove the feedback…
Part Number: TPS62133 Hi,
Can TPS62133 (5V fixed output) provide a regulated output when the input voltage is 5V? What would be the approximate output voltage considering the drop across mosfet and inductor?
Part Number: TPS62133 Other Parts Discussed in Thread: TPS62130A-Q1 , TPS62140 , TPS62140A , TPS62150 , TPS62130 , TPS62130A , TPS62150A Could you please let me know when this part will become available? Or could you suggest an alternate part that is…
Part Number: TPS62133 Other Parts Discussed in Thread: DRV8870 , On our PCB we plan to use the TPS61233 to generate a stable 5V (1A load) and motor driver DRV8870 (max. 2A load) sharing the same 12V input. Is there a risk that load changes on the DRV8870…
Part Number: TPS62133
Hello,
I am using the TPS62133 for a 5V / 2.5A supply. 5V_PSU.pdf
With no load, I measure 5V, howerver with approximately 250 mA, the voltage rail drops down to 4.6 V.
It keeps dropping down with higher current demand.
…
Part Number: TPS62133 At this moment we have designed a PCB for a customer where we use 3x TPS62133A for generating 3 different +5V supplies out of +12V. For the input we use a 10uF/25V/X7R/1206 cap in parallel with 100nF and at the output a 22uF/10V…
Hi Ian,
The TPS62133 and almost all DC/DCs (even most battery chargers) have current limit protection. So, the IC will protect itself by limiting its output current. You can read the D/S for an explanation of how the current limit works in this device…
Hi,
I have a very similar problem in my project with TPS62133: it fail without apparent motives.
Could you try to post the images with the micro crack?
Best Regards,
Fabio
well it looks like all is in order!
I was using an old datasheet (June 2013) for the TPS62133, at which there was a slight exposed thermal pad area difference.
Thanks,
Itay