Part Number: TPS62136 Other Parts Discussed in Thread: TPS62730 Hello All,
I would like to know what the most appropriate method is to create a BYPASS path for the TPS62136 buck converter? I would like to create a path where VCC is connected directly…
Part Number: TPS62136 Hello TI
The data sheet for the TPS62136 suggests that in order for the voltage output to be stable the total ESR of the cap bank can't get too low. For a power rail capacitance of >= 400 uF, it is recommended that that the trace…
Part Number: TPS62136 Hello, I was wondering what will be the best way to control 3 of this power supplies with the same or only 1 GPIO. Our application uses 3 of the TPS62136 to provide different power supplies rails and we would like to turn them on/off…
Part Number: TPS62136 Other Parts Discussed in Thread: TPS62135 , Hello Guys,
Good day.
Our customer is considering using TPS621361 as an alternative TPS62135. Note that he is initially considering TPS62136 but it is out of stock.
However he only have…
Part Number: TPS62136 Hello all, My application involves a battery and a DC load that needs to be operated between 0V-Vbat.
My battery voltage ranges from ~6V to 8.4V (it's a 2S lithium battery). The battery goes straight into Vin of the TPS62136.
…
Part Number: TPS62136 Other Parts Discussed in Thread: TPS62130 , Dear TI Team
I would like to ask about L value of TPS621361.
Our customers are trying to change the inductor value from 2.2μH to 3.3μH or 4.4μH to reduce the ripple current.
However…
Part Number: TPS62136 Hi,
Is it possible to be taught the fluctuation of output discharge resistance ? I want to know the min/max value roughly to design off-sequence.
Thanks,
Hayakawa
Part Number: TPS62136 Other Parts Discussed in Thread: TVS1400 , TPD2E007
Our customers are considering placing Zener diodes and resistors for the purpose of ESD protection for TPS621361. I would like you to answer the following questions.
1. Is there…
Part Number: TPS62136
Dear all,
Our customer is evaluating a sample to consider the TPS62361. Among them, when we confirmed the load characteristics from our customers, As shown below, when the load was increased, the switching frequency became faster…
Part Number: TPS62136 Other Parts Discussed in Thread: TPS7A8300 Hi team,
Customer is looking for the graph of TPS62136 θJA versus Board Size. Could you tell where we can get this?
I mean the figure 53 of TPS7A8300 datasheet as the example.
Regards…