Part Number: TPS62150 Other Parts Discussed in Thread: TPS562200 , , TPS62147 , TPS62148
Hi
We are evaluating TPS62150EVM-505 and facing problem of unwanted radiation noise.
Measured noise is attached in following file.
Input : 9V
Output …
Part Number: TPS62132 Other Parts Discussed in Thread: TPS62130EVM-505 , TPS62140EVM-505 , TPS62150EVM-505 ,
Hi, I'm creating my custom PCB using the TPS62132RGTR.
In the SLVU437A (TPS62130EVM-505, TPS62140EVM-505, and TPS62150EVM-505 Evaluation…
Other Parts Discussed in Thread: TPS62150 , TPS62150EVM-505 , TPS62150A Hi,
How can I get the TPS62150EVM-505 with TPS62150 A device on it?
The user guide of TPS62150EVM-505 (SLVU437A -October 2011 - Revised July 2013) mentions as below.
…
Part Number: TPS62150 Hi there,
My customer uses TPS62150 to convert 5.7 V to 5 V. They found that when there's no load, the transition between PWM/PSM varies with different switching frequencies.
I have the test results (with TPS62150EVM-505) summarized…
Ramgopal,
Your assessment of the bulk decoupling required is correct. You must calculate the required amount and validate it. The Hardware Design Guide (SPRABI2) discusses this calculation.
This bulk capacitance will affect the control loop on the…
SI,
Please see the attached presentation. It was originally prepared for the LM10010 which was later superceded by the LM10011 which has higher precision. Please also see the many E2E posts discussing the LM10011 and TPS56121 with C667x and C665x. …
tps62133.pdf Thanks for your support John. So sad to know there is no way to be informed when this type of changes happen!
Hi Chris,
Attached is the datasheet. I hope to have attached it correctly. Page 37 shows the old package drawing.
If you can…