Part Number: TPS62160-Q1 Other Parts Discussed in Thread: TPS62160 Hello,
I currently use the TPS62160 in WSON Packages by using the WEBENCH® Power Designer, and I would like to know if I can replace this component by 'TPS62160-Q1'?
And knowing…
Part Number: TPS62160-Q1 Hello Team,
The voltage reference of TPS62160-Q1 is given in the datasheet with 800mV typical at TJ 25°C. At room temperature 780mV was measured at the feedback node.
The total given output voltage tolerance is mentioned to…
Part Number: TPS62160-Q1 Dear TI,
We are using the TPS62160QDSGRQ1 step-down converter for supply to the Hercules uC core. The TPS62160QDSGRQ1 is automotive qualified, but not ISO26262, is there a set of failure modes/distribution and a FIT TI recommends…
Part Number: TPS62160-Q1 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hi Team,
I used Webench analyze the TPS62160-Q1, however, there is not a option to produce a bode plot to check stability for this device in Webench…
Part Number: TPS62160-Q1 Other Parts Discussed in Thread: TPS62150A Hi Team:
Customer use TPS62160Q1 in ADAS system.
The application is 5V input and 3.3V output. But they do an experiment that, change the input to 3V, which will make the input lower than…
Part Number: TPS57114-Q1
Hello
We are in a new design and in order to correctly evaluate the thermal behavior of the new design, we are carrying out some thermal simulations.
During the performance of these simulations, some questions have arisen about…
Hi Alex,
TPS62150A-Q1, TPS62160-Q1 or TPS62170-Q1 should work well here. I see you started an email chain on this topic as well so we can discuss there if any more questions.
Thanks,
Amod
Part Number: TPS62162 Other Parts Discussed in Thread: TPS62160 , TPS629210 , TPS629210-Q1 Hi,
Good Day. I have a customer who is working with TPSM84205EAB. Please see below his query for your reference. Thank you very much.
Due to the short supply of TPS62162DSGR…
Hi Tao,
1: Yes, you are right.
2: For fixed voltage version, the internal resistive feedback divider is included. That is for TPS62161/2/3 which is no external feedback resistor divider.
For TPS62160 output voltage calculation, please refer to datasheet…