Part Number: TPS62161 Other Parts Discussed in Thread: TPS62160 , , TPS61253A , TPS62293-Q1 Dear TI,
Can you please confirm whether the Two Ic's are compliance with Automotive standards.If not could you suggest an alternative with automotive grade.We need…
Part Number: TPS62160 Other Parts Discussed in Thread: TPS62161 , , Dear supporter, please confirm a question on DC output acuracy calculate.
1)normally DC output acuracy should consider FB acuracy and external resistor divider acuracy, am I right? i find…
Hi Kiran,
What is output voltage for your application? We have TPS62161 for 1.8V, TPS62162 for 3.3V and TPS62163 for 5V. Please refer to datasheet page4.
Thanks,
Nancy
Part Number: TPS62162 Other Parts Discussed in Thread: TPS62161 , Hello,
I have a 3.3V TPS62162 voltage regulator. It is sequenced by having a 1.8V TPS62161 voltage regulator connected to the Enable Pin. The power sequencing works correctly on power up…
Hi Linda,
Yes, that app note is a good find and should explain that the Cff does not usually affect the control loop since the BW is too high.
Only the TPS62161/2/3 have the internal resistors on the (internal) FB pin. The TPS62160 uses external resistors…
Hi V Pot,
Sorry, I missed your responses.
V Pot said:
1)Anyways we gonna make a pcb with just c5545 , aic3206. So you are confirming that c5545 dsp has a i2s3 to use for transmitting to the micro processor?
Yes, the C5545 has an I2S3 that you can use…