Part Number: TPS62163 Other Parts Discussed in Thread: TPS62153 hi, experts
When using the TPS62163 with VOUT = 5 V and IOUT = 1 A, what is the minimum allowable input voltage for stable operation?
Part Number: TPS62163 Other Parts Discussed in Thread: PMP41042 Hi TI team
I have a little confusion about VT-22247A used in PMP41042. The transformers' core is PQ52/32/43.8. It seems like the power rating is<1kw, but it was actually used in 3.3kw system…
Part Number: TPS62163 Tool/software: Hello,
I am trying to solve this issue within the DRC for Altium PCB Editor (issue is this error: Routing Via Style: Via (1584.646mil,2601.541mil) from Top Layer to Bottom Layer Actual Size : 19.685mil Actual Hole…
Jose,
TPS62163 is capable of 100% duty cycle operation, so input voltage of 7 V should not be a problem. There is one item that may be an issue. L504 is a physical inductor. It may cause ringing on your input with excessive ripple on the input. Can…
Part Number: TPS62163 Hi team,
I see there is a Initial output voltage accuracy data in the datasheet. I'm not very sure what the data mean here. Is it the accuracy of the internal reference voltage?
Part Number: TPS62163 Other Parts Discussed in Thread: TLV62130A Hello,
I have a question for TPS62163 regarding output discharge function.
TI.com's list of DCDC said TPS62163 has output discharge function. However there is not on datasheet. …
Part Number: TPS62163 Other Parts Discussed in Thread: TPS62162 I cannot find the drop-out voltage in the spec. It says that it'll run up to 100%, which implies a very low dropout voltage, approaching 0. I need a 5V supply with a Vin down to 5.5V. I would…
Part Number: TPS62163 Other Parts Discussed in Thread: TPS62150A Hi,
Does TPS62163 have output discharge function?
I found "Outout discharge" wrriten on ESP,but it was not written in block diagram.
Could you tell me about this?
Best Regards…
Part Number: TPS62162 I have been having odd problems with my two VREGs, this is related to the post I made previously. Anyways, my layout was not the problem, which was a theory I was little skeptical of given the symptoms. I assembled my new board and…
Hi Lakshmi-san,
Thank you for your reply.
I changed the TPS62163 transient model (slvma51) and designed a circuit like the attached TSC file.
TPS62163_inverting.TSC
As a result of simulation with this circuit, it looks like the following image…