Other Parts Discussed in Thread: TPS62163 Hi,
I download the TI TPS62163_DSG CAD file and check the file using ULADICIS tool.
But the file is not WSON 8pin package at TI website.
Please kindly help to check where is right download link.
Thanks.
Part Number: TPS62173 Other Parts Discussed in Thread: TPS62163 Hi,
Customer wants to use TPS62163DSGR as a drop-in replacement for the TPS62173DSGR. Looking through both data sheets it looks like the only difference between the two is maximum output current;…
Other Parts Discussed in Thread: TPS62163 HI
I would like to use the TPS62163 with Input Power 6-17V and 500mA-900mA with 5V Output (for sensors). I'm expecting quite a lot of noise. Noise reduction is far more important than transient response.
…
Other Parts Discussed in Thread: TPS62163 , TPS5450 I use a TPS62163 (L: 2.2µH, Cout: 2x 10µF) to generate 5V for USB port from a 11.8V rail.
We got resports of some USB stick failing in the field after been used with this power.
I inspected one…
Hi Kiran,
What is output voltage for your application? We have TPS62161 for 1.8V, TPS62162 for 3.3V and TPS62163 for 5V. Please refer to datasheet page4.
Thanks,
Nancy
Hi Francis,
Please find my reply below.
1. The heatsink were custom parts, so do not have a ordarable part for them. Larger heatsinks are only for thermal reason at full load and minimum battery voltage condition. However you can reduce the size depending…
Part Number: TPS62162 Other Parts Discussed in Thread: TPS62163 , I am currently powering the the SAMC21 in dual power supply mode with the 5V TPS62163 and the 3.3V TPS62162, the 5V IC is working fine, however the 3.3V IC is outputting 3.66V(very stable…
Selva,
I've reviewed your schematic and layout.
One thing I've noted from your schematic is that there are no 100k pull ups on pin55 (UART_TX) and pin57 (UART_RX).
From your layout:
1) From looking at your Top Solder mask gerber file, it looks…