Other Parts Discussed in Thread: TPS62163 , TPS62160 Hello,
I`m interested in TPS62160 / TPS62163.
Is it possible to see how old the dc/dc Converter is and if it is recommended for new designs?
Thanks in advance
S. Hilgers
Hello again,
I've settled on the TPS61170 for the +35Vdc supply and the TPS62160 for the +5Vdc (well, actually a TPS62163 for the +5Vdc and a TPS62160 for a separate 5.7Vdc).
However, with a slight shift in the input voltage specs (Vin could be …
I'm having the same issue, although I'm trying to use TINA-TI to simulate a TPS62163 . I'd also like to get the TPS62133, TPS2115A and LM3410 converted to work with TINA-TI as well if possible.
Other Parts Discussed in Thread: TPS62112 , TPS62143 , TPS62163 , TPS62141 Hello,
I would like to use the TPS62112 in my new design. The user is offered 2 options to power the module:
- Using 12V which is converted to 5V using the TPS62112
- Using 5V directly…
Thank you for including your schematic, PCB layout, and waveforms. Your schematic looks ok. Improvements in the PCB layout include a closer GND connection of the input and output caps to the PGND pins and a thicker trace connecting to the inductor. You…