Part Number: TPS62170 Other Parts Discussed in Thread: TPS62160 , TPS62125 For the TPS62170 (and also the TPS62160) , the vout max is listed as 6V. What is driving this limitation? Is there a work-around to get 9V output (with say, 12V input)?
The device…
Part Number: TPS62170 Other Parts Discussed in Thread: TPS62065 , Hello Support team,
In case of TPS62065, the output voltage has 1% gap between PWM and PFM according to datasheet below.
I guess that TPS62170 may have similar output voltage gap between…
Part Number: TPS62170 Other Parts Discussed in Thread: INA210 , Hi!
In my application I need to measure the current at the output of the converter, for that I have a resistor and a INA210.
The resistor will produce a voltage drop, to correct that drop i…
Part Number: TPS62170 Hi team,
Can you answer the following customer inquiry?
I have a question about the switching regulator TPS62170. In a circuit it is used to convert +3.4 V to +1.8 V. During measurements in Power Safe Mode (output current about 50…
Part Number: TPS62170-Q1 Other Parts Discussed in Thread: TPS62170 , HI Team,
My customer is using the TPS62170, but the current can be up to 600+mA sometimes. Is there any risk on this?
I check that datasheet mentioned 850mA is the current limit. However…
Part Number: TLV767 Other Parts Discussed in Thread: TPS62170 , How is the variation of the VREF over the temp range?
In the E/C table, it only specify the 0.8V,typ value. Thanks.
Regards
Brian
Part Number: TPS62170-Q1 Hi, we built 20 samples of car camera this week, and found one piece sample the SW waveform is abnormal during power up (refer to Vsw in Figure 1). This symptom can be disappeared (refer to Figure 2) when we wait for a few seconds…
Part Number: TPS62170-Q1 Other Parts Discussed in Thread: TPS62170 Hi team,
My customer uses TPS62170 in camera module. There is a project they use this part to 8->3.8V@150mA stage.
The issue is 1/5 cameras has ripple in the display. Other cameras…
Part Number: TPS62170 Hi Team,
Recently my customer is designing the TPS62170.
Input: 4-16V. typ: 8V
output: 3.5V, Iout max: 0.3A.
Based on the webench design, I can get below design. for the feedback resistor, it suggested: 180k & 604k.
However…