Part Number: TPS62175 Hello.
I have a question about TPS62175.
What is the maximum frequency of the switching frequency? There is an IC that operates at 1.7 Mhz.
Thank you.
Part Number: TPS62175 Other Parts Discussed in Thread: TPS62160 , TPS62125 , LMC6482 Hello all,
I am with a project that needs a negative voltage and have chosen the TPS62175. For the non-inverted (normal) configuration
there is an example in the datasheet…
Part Number: TPS62175 Hi,
Good morning!!
We are currently using TPS62175 switcher for converting 24V DC to 5V supply for our design we are facing Emission issue at 614KHZ in Radiated electromagnetic disturbance 44dBuV in Y and Z axis as per EN55015, I…
Part Number: TPS62175 Hi,
The datasheet is described that VOUT rises with a slope of typically 10 mV/µs.
How much is the dispersion of this rise time?
I would like to know for our reference, and do not require the guarantee.
Best Regards,
Kuramo…
Part Number: TPS62175 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Where can I get an unencrypted version of TPS62175_TRANS PSpice model?
Other Parts Discussed in Thread: TPS563201 , TPS62175 , TPS54525 , TPS62150A , TPS62160 Following the suggestion of Webench, I used a TPS563201 to step down from a +12V supply of a PCIe connector to an intermediate voltage +7V before finally reaching the desired…
Other Parts Discussed in Thread: TPS62175 I have come across an interesting problem using the TPS62175 as a stepdown regulator from a battery input. The situation is as follows: The TPS62175 is being fed from an 8.4V (max) lithium-ion cell pack. I am using…
Hey Chris,
thanks for your help. I don't want the storage cap on the input rail, because i need an 25V volt capacitor, otherwise i can use 6,3V type.
My solotion is to put the capacitor behind a tiny load switch, so i can use the full 5V. In case…
Hi,
If I calculate the Lmin using the formula in datasheet with Vout = 5V, Vin(max) = 10.5V, delta IL(max)=0.009 A (0.03A is load current), Efficiency = 0.9 (90%) and Fsw= 183856 Hz (Web bench simulation)
I am getting Lmin = 0.001581 Henry(As per calculation…
Other Parts Discussed in Thread: TPS62175 Hello,
I built a product using the TPS62175 step down regulator. The prototype is not working and I don't understand why. Can you help me find the problem?
Cin: 10uF/50V MLCC
Cout 47uF/16V MLCC
Lout: 10uH …