Part Number: TPS62177 Hi,
I am using TPS62177 switcher in my design. The maximum load current is around 100mA. Is there a requirement to add snubber circuitry at the switching node for EMI/EMC considerations?
Part Number: TPS62177 Other Parts Discussed in Thread: TPS62175 Hello Team,
is it possible to get a little higher Vout like 3.5V instead of 3.3V with the TPS62177 by connecting an R-divider from Vout to the Vos-pin?
Thanks and Best Regards,
Hans
Part Number: TPS62177 Hello,
I have a question regarding the use of the "Sleep" Pin for the TPS62177.
In the datasheet I saw that if a high current is pull when the device is in sleep mode, as a safety feature the device return to normal operation…
Part Number: TPS62177 Other Parts Discussed in Thread: TINA-TI ,
Tool/software: WEBENCH® Design Tools
Hello Team,
if I do a Webench Simulation for TPS62177 I see Vout = 3.3V which is expected. Using the "Sim Export" button to create a TINA-TI design…
Part Number: AM2434 Other Parts Discussed in Thread: TMDS243EVM , UNIFLASH , TPS62177 , I am trying to flash TMDS243EVM using mcu_plus_sdk_am243x_08_06_00_45. However, writing fails as shown in the screenshot. Using the same script to burn TMDS64GPEVM is successful…
Part Number: TPS62177 Hi guys,
This question might be trivial, but nevertheless something I need to know.
I'm using the TPS62177 for a 13V5 to 3V3 step-down conversion which is supplying MCU etc.
For J-Tag programming of a MCU (during production test…
Part Number: TPS62177
Hello Folks,
Would be grateful for some suggestions as to how best to explore and resolve this issue. This is a new design for us, and our first use of this part. The enclosed schematic (in PDF) could not be simpler in terms of…
Part Number: TPS62177 I am using the TPS62177 in a standard 14-16VDC input to 3.3VDC fixed output topology. I have noticed an issue where around 14.25VDC on the input, the output voltage begins to climb. Our primary input voltage is 15VDC. The measured…