Part Number: TPS62290 When the MODE pin of the TPS62290 is set to LOW, automatic switching mode is enabled. What is the minimum threshold current for switching to PWM mode in this mode?
Part Number: TPS62290 We are using the following components in our design:
SN74AVC2T245RSWR,
TCA9803DGKR,
ADS112C04IRTER, and
TPS62290DRVR.
Could you please provide the MTBF/FIT data (or MTPF files, if available) for these parts? This is…
Part Number: TPS62290 Tool/software: Hello, My customer built their own prototype with TPS62290. Then they found MODE pin is wrongly left floating. Does it have internal pull-up or pull-down? They are wondering if they absolutely have to modify the board…
Part Number: TPS62290 Tool/software: Hii Team,
We are in Requirement of CE Certification details for the below parts, please provide info on this
TPS62290DRVT
TPS73701DRBR
TPS62291DRV
SN74LVC1G34DSFR
Regards,
Karthik
Part Number: TPS62290 Tool/software:
We are observing an issue where the input and output voltages are the same. We have cross-verified the feedback (FB) resistor network and performed impedance testing.
We also probed the SW pin using an oscilloscope…
Part Number: TPS62290TPS62290 problem.
My design has TPS62290 as '5V->3.3V converter'. It's well running and there is no problems, even in very high temparture test.
But when I touch the top of the chip(62290), it's going to very high temparature…
Part Number: TPS62290 Dear Teams,
Could you help check following question from my customer?
Problem: As the power input VBUS dropped from 5V to about 2.2V, the output of TPS62290DRVT changed from normal 1.15V to about 2.9V, which caused serious load…
Part Number: TPS62290 Hi,
Good Day. I have a customer who is working with TPS62290. Please see below his query for your reference. Thank you very much.
our application needs around 100mA of load current in maximum
so i calculated the inductor…