Part Number: TPS62404-Q1 Other Parts Discussed in Thread: TPS62404 , , TPS62400 I’m currently using the dual buck converter IC from TI (TPS62404QDRCRQ1) that is supposed to output 1.575V and 3.3V. The 3.3V output (Vout2) is working fine. However, I measured…
Other Parts Discussed in Thread: TPS62402 , TPS62404 , TPS62400 Hi,
I would like to use a TPS62402 or TPS62404 with Vout1 set to 2.8V or more. It should be possible to insert a resistor between Vout1 and FB1 to achieve this. It is easy to compute this…
Hi,
wayne lu1 said:
Although I still need to use power line to transmit the data about the motor's speed or something else to control the motor.
So, do I need to buy a new device or any software I can use?
if you wish implement motor control…