Part Number: TPS62442-Q1 Tool/software: Hi, experts.
I plan to use TPS62442-Q1 to step down 5V to 1V,as shown in the manual, the maximum frequency for converting 5V to 1V is 2.67 MHz.
To enable the SSC function, I connect the COMP pin to VCC , does…
Part Number: TPS62442-Q1 Tool/software: Hello team,
Hope you are doing well.
My customer wants to replace Maxim 3-channel buck to our TPS62442-Q1, but not sure about the current capability.
The two channels' requirements are separately 3V3->1V(1…
Part Number: TPS62442-Q1 Hi TI Team,
We are planning to use TPS62442-Q1 in our automotive design, and we tried to simulate the TPS62442-Q1 Pspice model provided in the TI site.
But failed to simulate the output voltage of 1.8V as designed in the…
Part Number: TPS62442-Q1 Other Parts Discussed in Thread: LM26420-Q1 , Hi Friend ,
AS LM26420-Q1 Spec, I can find the DMAX just below the pic . but I can't find the same parameter in the TPS62442-Q1. so can you give me this parameter of TPS62442-Q1…
Part Number: TPS62442-Q1 Tool/software: Hello, The features of this device shows "2 × 2-A or 3-A and 1-A output current" in the datasheet. I'd like to know what factors determines " 2 × 2-A output mode" or "3-A and 1-A output mode". Please let me know…
Part Number: TPS62442-Q1 Other Parts Discussed in Thread: LM64460-Q1 Hi,
I am designing a DC-DC buck regulator with 3.3V input and 2.5V and 1.2V as outputs, I have used TPS62442-Q1 and followed the WEBENCH design for this. I also need this circuit to…
Part Number: TPS62442-Q1 Hi,
My customer is looking at using the TPS62442-Q1 for a dual output application but they are concerned about EMC. Can you provide more details about the phase shifted operation and how SS works with the phase shifting feature…
Part Number: TPS62442-Q1
before the device start, the output shart like RC curve, and when shut down EN pin, the output is still on about 300mV. could you explain why? and detail reason
Part Number: TPS62442-Q1 Hi Team,
I want to use the transient model to do the loop test.
The result is incorrect.
Can transient models be used for loop testing? Or are there any mistakes in my loop test model?
Thank you!
Part Number: TPS62442-Q1 Hi Team,
I want to use the transient model to do the loop test.
The result is incorrect.
Can transient models be used for loop testing? Or are there any mistakes in my loop test model?
Thank you!