Part Number: TPS62733 Other Parts Discussed in Thread: TPS62730 The Docs always refer to 2 cell alkaline, not one. Can this work with a single?
Also, the TPS62733 came recommended, however, at 2.1V, the ADC on my MPU430 requires 2.2V min which is higher…
Other Parts Discussed in Thread: MSP430F2481 , CC2540 , TPS62730 Hello;
I had a circuit with msp430f2481 and a BLE112(cc2540 wit 8051) module.Communication between the two modules is done through UART.so far so go,my module works fine.
but for reasons…
Part Number: CC2540TPS62730EM-RD Other Parts Discussed in Thread: CC2540 , TPS62733 Hi
Actually, I am using a Li-ion battery of 4.2V as source for TPS62733 LDO with CC2540.
So LDO has 2 modes
1) It gives 2.3V as output
2) It gives Vin as output…
Other Parts Discussed in Thread: TPS62733 , CC2540 , CC2541 , TPS62730 , TPS61200 Hello,
I'm working on a Bluetooth low energy application based on a BLE112 modem, and MSP4302416 processor. As described in BLE112 datasheet, we have had a TPS62733 regulator…
Other Parts Discussed in Thread: TPS62730 , CC2541 , TPS62736 , TPS62733 , TPS62743 Dear TI' Engineer,
According to TI's reference, TI recommand TPS62730 to be the power supply of CC254x.
I use TPS62730 to power the CC2541, the TPS62730 output is…
Hi Di Wang1,
Input voltage range is 2.1V-3.1V. Output voltage is labeled: VDC-2V7.
Is output voltage 2.7V?
What is acceptable variation of the output voltage?
What is maximum output current for application?
The part number TPS62730 is…
I experimented with removing a 2.2uF cap near the cc2541(copied from the reference design), and I saw similar results regardless of the rise time. Page 20 of the TPS62733 datasheet says "The total capacitance of these decoupling capacitors should be kept…