Part Number: TPS62743 Hi, Is there a problem to connect VSEL1-3 and EN to VOS in order to get 3.3V of output?
The fact is, in PCB design, I prefer to make a clean design of the inductance between SW and Vout not tracing a track below that inductance. …
Part Number: TPS62743 Other Parts Discussed in Thread: TPS62745
Hi! I use TPS62743 in li-ion battery-powered application. Supply current 12uA in sleep mode and 8mA in active mode. Vout programmed to 3.0V.
Cin 4.7uF Murata GRM188R61E475KE11
Cout 10uF …
Part Number: TPS62743 Other Parts Discussed in Thread: TPS62840 Does TPS62743 has thermal protection and over current protection?
If yes, what is the protection temperature and protection current? I can't find them in the spec.
Thank you!
Part Number: TPS62808 Other Parts Discussed in Thread: TPS62743 , , TPS62840 Hi! Currently, I'm using TPS62743 to convert 5 V to 1.8 V to power a BME680 which has a peak current of 12 mA during the measurement. Because I can only draw 5 mA at maximum…
Part Number: TPS62743 Dears
I have been using this material for a long time, and there is no problem.
Recently, the production factory reported that there were problems with these two plates:
the material tape was too sticky, it was not easy to separate…
Part Number: TLV627432 Other Parts Discussed in Thread: TPS62743 , Dear Engineer
Is there any difference between TLV627432YFPR and tps62743?
From the datasheet, there is almost no difference. Pin2pin, the output current is 400mA, the voltage level is the…
Part Number: TPS62743 Dear E2E Support,
My customer is facing some noise issue in his application using a GPS ; which limits the performances of it.
1- is there any limitation to use our TPS6274x family to directly power a GPS?
Note that in our case…
Part Number: TPS62743
Hi team,
My customer is using TPS62743 in their project. In this design, VIN is from 4.2V battery and TPS62743 is configured 3V output for feeding to MCU ONLY.
The RD found when set VIN from 4.2V to 2.8V, the current consumption…
Part Number: TPS62743 Other Parts Discussed in Thread: TPS62746 , TPS62748 , TPS62770 , TPS62808 Hello,
Interested in 1.8V for a low power battery design but I'm a bit confused.
If I look at the datasheet for the TPS62743 and examine table 1 I see that…
Part Number: TPS62743 Other Parts Discussed in Thread: TPS62748 , TUSB542 Hi Team,
I am creating a design with a step down from 3.3 V to 1.8 V and am looking for a part recommendation. I am currently looking at the TPS62743 vs the TPS62748. I am trying to…