Part Number: TPS62745 Tool/software: Hi Experts,
What is the minimum enable voltage threshold for the EN pin on TPS62745DSST? I cannot find it in the datasheet.
Regards,
Marvin
Part Number: TPS62745 Tool/software: Good afternoon,
I have a battery powered product ( 6 X AA, Max. Input voltage 9.6V) that carries two TPS62745 regulators for generating both 1.8V and 3.3V for the main MCU. 1.8V is for core supply while the 3V3 is…
Part Number: TPS62745 Tool/software: Hi expert,
Do we have the data which shows max. Iq at room temp(25C)? My customer would like to know this.
Regards,
Kotaro Yamashita
Part Number: TPS62745 Other Parts Discussed in Thread: TPS62840 , LMR43610 Tool/software: Hi team,
My customer is considering a power IC for input to a microcontroller from 4 batteries in series .
Please introduce a DC-DC converter that meets the…
Part Number: TPS62745 Other Parts Discussed in Thread: TPS629203 Hi Team,
Is any better device being available compared to TPS62745?
High level Requirements:
Input voltage range= 2.7 to 15V
I out current = 250 to 300mA
V out voltage =3.3V…
Part Number: TPS62745 Hi Team
I’d like to ask about MSL of TPS62745DSSR.
This time, MSL1 and MSL2 products were delivered to our customer.
We confirmed that the latest data sheet has an MSL of 1.
However, there was no history of a PCN being issued…
Part Number: TPS62745 Tool/software: I had tested and confirmed it in a different board with a current source, but I had manufactured the same in a new board but it is not working properly.
My issue is like if I connected the regulator board to my base…
Part Number: TPS62745 Hi ,
Is there a replacement part for TPS62745 with same packaging and pin compatibility but input voltage level greater ( preferably Vmin = 6V and Vmax = 16 V ) with programmable output like that of TPS62745 ?
With regards, …
Part Number: TPS62745 Hi Team,
We have designed TPS62745 chip as per data sheet , all VSEL1 to 4 lines connected to VOUT Line. When I used TI ‘WEBENCH design tool‘ found all VSEL 1to 4 lines connected to VIN. PG is open in datasheet application ckt…