Part Number: TPS62745 Other Parts Discussed in Thread: TPS629210 , TPS629210-Q1 , In my application below are input / Output requirement.
Application = Battery operated LORA asset tracking pulsed load kind of application.
Vin = +7.2V(2S LiSoCl2 batteries…
Part Number: TPS62745 We have requirement where we need to convert +3.3V from 2 batteries of LiSoCl2 in series connection.
Combined voltage of series connection of 2 nos LiSoCl2 would be +7.2V and need to convert +3.3V from this.
Output Current requirement…
Part Number: TPS62745 I can't find any inventory for this part and it is holding up production - could someone help me get a hold of this part or figure out when they will be available to order? I'm currently held up in production because of this…
Part Number: TPS62745 Hi team,
The input voltage drops to about 3.1V at startup. Since it is below UVLO, will the device not start up? Sincerely. Kengo.
Part Number: TPS62745 Hi team, I'd like you to check my customer schematic. This device is generating a negative voltage, so please take a closer look. If it OK, can I talk offline?(Private message/e-mail) Sincerely. Kengo.
Part Number: TPS62745 Other Parts Discussed in Thread: TPS62125 , TPS62170 Hi team, When does the Discharge function work after UVLO? When the Discharge function is activated, the voltage of the output drops sharply. Is there a way to smooth this out? Sincerely…
Part Number: TPS62745 Hi team, I have confirmed before about negative power generation on the bellow thread.
My customer wants to change input voltage 8V from 3.3V. Is it okay to think that the input voltage is 11.3V because the output is -3.3V(negative…
Part Number: TPS62745 Other Parts Discussed in Thread: , TPS62125 Hi team, I'm looking for a device with a lower IQ that TPS62745. My customer condition is VIn=10V. Could you please introduce us including the developed products? Sincerely. Kengo.
Part Number: TPS62745 I am using the TPS62745 in a low current design, and every so often, I get a large (> 5mA) current spike. The period of the spike seems to shorten as load increases. Also, over multiple units, the period varies. I suspect the…