Part Number: TPS62801 Good day, colleagues,
In the production test my customer would supply from the test system a voltage (0.9 V) at the output of the TPS62801 while the VIN is not supplied . The 0.9 V corresponds to the output voltage setting by the…
Part Number: TPS62801 Other Parts Discussed in Thread: TPS62088 , TPS628503 , TPS628511 , TPS628513 , TPS628501 Tool/software: Hi expert,
Customer is looking into some of our power sequencing and have a question regarding the Logic Interface EN on two…
Part Number: TPS62801 Tool/software: Hello team,
Are there any major risks associated with using an inductor > 0.82uH (say, 2.2uH) in order to reduce ripple with the TPS62801.
Best,
Austin Allen
Part Number: TPS62801 Hello team,
My customer is in need of information on the UBM (Under Ball Metallization)/SRO (Solder Resist Opening) of this device TPS62801YKAR.
Thank you,
Austin Allen
Part Number: TPS62801 Hi Team,
I am wondering if the EN pin can be floating for about 10s on each start-up operation? Will it cause some reliability risk?
Thanks.
Sincerely
Frank
Part Number: TPS62801 Other Parts Discussed in Thread: TPS62802 Can you share me the expected values of below parameters for TPS62801 and TPS62802 ?
1. TON and TOFF.
2. Duty Cycle.
3. Ripple Frequency and Ripple Voltage range.
Part Number: TPS62801 Other Parts Discussed in Thread: TPS62802 , TPS62807 Hi team,
Customer is using TPS62801 -> 1V/15mA, TPS62802 -> 1.8V/15mA, input is Li-battery, 3V ~ 4.4V. Since their current output is very small, so they wander if they could…
Hi Franck,
The device is characterized and tested for the recommended condition in the datasheet. If the supply voltage is lower than the specification it will affect the performance of the device like load transient measurements, voltage drop, and…
Part Number: TPS62801
Hi,
TPS62801 VSEL/MODE pin is multi function
We can use external resistor to select output voltage(16 selectable Vout).
After power up (VSEL→MODE), the pin is configured as an input for Mode Selection.
Low level at…
Part Number: TPS62801 Hi, TPS62801 support team.
I would like to know the relation between "Operating Junction Temperature of Absolute Maximum Rating and Thermal Shutdown Temperature.
When comparing the above data, Thermal Shutdown threshold is…