Part Number: TPS62810M Hi,
This is Dinesh Bala Surya from iWave Global. We are planning to use this TPS62810MRWYRNEP part in our project. In that, copuld you please clarify whether can we connect the PG pin to input voltage instead of output voltage…
Part Number: TPS62810M Other Parts Discussed in Thread: TPS62810 If the spice model for the TPS62810 is unencrypted, why is the Simplis model encrypted? Having a full version of Simplis 8.1 isn't working.
Part Number: TPSM8287A12 Other Parts Discussed in Thread: TPS628304 , TPS62810M , TPS62827A , TPS62A04AB Dears,
Customer wants to use a higher frequency switching power supply, but the conducted noise will be greater. How to effectively suppress it…
Part Number: TPS54680-EP Other Parts Discussed in Thread: TPS62810M , TPS54380 , TPS628511 , TPS628501 Hello,
Wondering if there's a minimum load requirement for the TPS54680-EP?
The plots show efficiency down to 0.5A, but will it operate with a lower…
Hello,
thanks for reaching out in E2E.
I think the TPSM82810 would be a suitable alternative to the EN6347QA. But the maximum recommend input voltage is lower for the TPSM82810 (6V instead of 6.6V of the EN6347QA).
The TPSM82810 is only available…
Part Number: TPS54316 Other Parts Discussed in Thread: TPS62810M I am designing a 3.3V regulator solution with the TPS54316MPWPREP. Our FPGA will control the enable signal on the regulator so that it becomes enabled only when the ambient temperature read…
Hi,
Thank You for using E2E.I have listed below three options to power the Xilinx FPGAs. Let us know if you have any questions or need additional information.
TPS65219 + discrete : This option uses our newest cost/size optimized PMIC. We are…