Part Number: TPS62811-Q1 How do you recommend to achieve 0.6V out? The datasheet doesn’t give an example.
How can I implement the Cff? Can I just populate R1 with 20k, add Cff=10pF in parallel, and no-stuff R2?
Thanks, Alan
Part Number: TPS62811-Q1 Other Parts Discussed in Thread: TPS62810-Q1 Hi Sir,
My customer is asking if we have NoneQ version TPS62811?
the reason is that some of their end customer might need Q-grade and some might not need.
Thanks,
Patrick
Part Number: TPS62811-Q1 Hi team,
I'm looking for an automotive device of Vin=3.3V / Vout=2.95V. TPS62811-Q1 looks to be available.
Can you confirm if it's okay with TPS62811-Q1?
- VIN = 3.3V
- VOUT = 2.95V
- IOUT =1A
Thanks,
Sam Lee
Other Parts Discussed in Thread: TPS62813-Q1 , TPS62811-Q1 Hi,
Below is the table which includes of current requirements and corresponding datasheet requirements. Could you please suggest the alternate for below mentioned Part number (MPN) at lower price…
Part Number: TPS628502-Q1 Other Parts Discussed in Thread: TPS62811-Q1 Hello Expert,
I'd like to confirm about the risk of glitch on PG pin when I pulled-up PG pin to output of TPS62811-Q1 itself.
I think, PG pin's deglitch time is less than 1us and…
Part Number: TPS62811-Q1 Hi team,
May I know if TPS62811-Q1 need to add RC snubber from SW pin to GND or not?
If snubber can't be used for this device, to reduce SW node spike of TPS62811-Q1, as I know besides input 0402 MLCC decoupling cap, any ways…
Part Number: TPS54719 Other Parts Discussed in Thread: TPS62811-Q1 , TPS628501 Hi,
We are using the TPS54719RTER buck converter for 1.8V and 1V for our application having two FPGAs (XC7S50-1FGGA484C, Spartan-7 series ).
Following is the requirement,
For…
Hello Rackshith,
I had similar discussion with our colleague in Bosch on how to calculate for the worst-case IC power dissipation using Webench. Please refer to the link below for reference.
https://e2e.ti.com/support/power-management-group/power-management…
Part Number: TPS62813-Q1 Other Parts Discussed in Thread: TPS628501-Q1 , TPS62811-Q1 Hi Expert,
Could you please check if the output inductor is proper?
From the data sheet, recommended MAX inductance is 0.9uH.
But the customer design target are
Vin…