Part Number: TPS62813-Q1 Hi,
Background:
I am using this IC in our application. This IC is mounted on the PCB and enclosed with aluminum Housing.
Can I consider temperature inside the Housing as Ambient Temperature here or should I consider temperature…
Part Number: TPS62813-Q1
Hi Sir,
5V to 2.5V, Imax=0.6A
For EMC consideration, we put 100uf POSCAP and 47uf MLCC*2 on the output.
When we start the system, we will see abnormal overshoot and then we remove the 100uf POSCAP and the overshoot phenomenon…
Part Number: TPS62813-Q1 Hi Team,
As title, do we have recommended max phase margin? About below two result, which one do you suggest? (Cff = 10pF vs Cff = 100pF)
Regards,
Roy
Regards,
Roy
Part Number: TPS62813-Q1 Hi,
I am working on worst case calculation. I couldn't find the parameters like dead time, gate charge/ capacitance, gate drive voltage, body diode forward voltage (can it be assumed 0.5V?) in the datasheet. Could you please…
Part Number: TPS62813-Q1 Other Parts Discussed in Thread: LM63635-Q1 , TPS62870-Q1 Hello,
We are having a requirement as below:
Buck Converter 1 -
Input Voltage: 4V to 5.5V
Output Voltage: 3.8V
Output Current: 3A-3.5A
Buck Converter 2 -
Input Voltage…
Part Number: TPS62813-Q1 Other Parts Discussed in Thread: TPS62813 Hi Experts:
I have used the model downloaded form TI to simulate. But when I have changed the runing time to 1s and maxing shep time to 1ms, and then why is the result of Vout outp…
Part Number: TPS62813-Q1 Other Parts Discussed in Thread: TPS628501-Q1 , TPS62811-Q1 Hi Expert,
Could you please check if the output inductor is proper?
From the data sheet, recommended MAX inductance is 0.9uH.
But the customer design target are
Vin…
Part Number: TPS62813-Q1 Other Parts Discussed in Thread: TPS62813 , LM73606 Hi,
TPS62813 : Vin=5V and Vo=1.1V or 1.8V
The input voltage of TPS62813 is from the output of LM73606 (LM73606 12Vin to 5Vout)
Both of LM73606 and TPS62813 EN signal are tied to the…