Hi, There was no feedback since a while, so I assume this tread is resolved and can be closed. You can still reply to this thread after it is closed, or you can create a new thread. Best Regards, Andreas.
Hi team,
EN pin should be pulled high or low?
Kindly verify the design of buck regulator for 1V1 & 1V2
Lets know the inputs from you.
Thanks,
Sathya Priya N
Part Number: TPS62826A Other Parts Discussed in Thread: TPS62826 , Hello team,
I have a contact who is evaluating both the TPS62826A and the TPS62826 (non-A version). They are seeing differences in the voltage swing between the two devices as shown bel…
Part Number: TPS62826A Other Parts Discussed in Thread: TPS62866 Hi team, When is CSP PKG for the TPS62826A and 5A release? Currently only QFN. Sincerely. Kengo.
Hello Kristina,
this thread seems to be duplicate to another thread: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1431247/tps62826a-dip-occurring-on-the-en-line .
I will close this thread and continue the…
Hi Andreas,
Is that TLV62085 having the FPWM mode? (If yes then what do we need to change in the hardware) Because the TPS62826A or the TPS628303 is not footprint-compatible with the TLV62085.
Hello Roberto,
thanks for using E2E.
The chosen inductor value is quite large compared to the typically suggested values of 2.2uH ...10uH (see design guide ).
The ESR of the output capacitor has an impact on the ripple voltage (see Equation 8 in the design…
Part Number: TPS62826A Hi Team,
Can you review the below design is fine for 1V1 and 1V2 using TPS62826ADMQR buck regulator.
Let us know the decaps provided are sufficient.
I attached the image for the reference.
Thanks,
Sathya Priya N
Hi Peter,
For this particular case, TPS62826A are production material (RTM version), although it was built under SWR. And it meets all the datasheet specs. Anyway, the SWR sticker should not be placed in the packaging.
I hope I was able to answer your…