Part Number: TPS62825 Other Parts Discussed in Thread: TPS62827
Hi, Could you tell me about the efficiency of TPS62825/6. I believe that the efficiency curve shown in datasheet P.14 is TPS62827. And I understand that the deference between TPS62827 and TPS62825…
Hi Aki,
The TPS62827 is a 4A, low Iq device in a much smaller package.
If you need further support for your specific customer, contact me with an email.
Hi Lalit,
For a 5V input, the TPS62827 is like the TPS62085 and can be used.
For 12Vin, the TPS62136 is similar and can be used.
For powering the VEE rail on the DAC, please see TPS63710. With its 1A output, it should be able to power all 3 DACs. …
Part Number: TLV62095 Other Parts Discussed in Thread: TPS62827 Hello Sirs,
We want to Vo 0.9V and 0.75V switch with a parallel resistor
Feedback R up is 80.8K
Feedback R down is 1M ohm // 1M ohm
Is there problem to use such large resistor for tlv62095…
Thanks Bren.
Yes, the TPS6282x family is recommended for new designs. It is a higher efficiency, though larger, option for LPDDR4. The TPS62826 offers a pin to pin upgrade to 4A, if needed, with the TPS62827.
The details of our customer's DDR loads…