Hello Yasuhiro Takemoto,
As mentioned before, TLV62090 is very old device and back then, this data is not characterized with the requested condition(VIN ≦ VOUT + 1).
I would recommend to look into our newer devices in which you can find output accuracy…
Hi Devipriya,
We don't have a higher current dual buck. Would 2 single rail devices work for your application? The TPS628303A is available in a 1 x2mm QFN package. https://www.ti.com/lit/ds/symlink/tps628303.pdf
Best regards,
Varun
Hello Foong Wei Seng,
Thank you for reaching out,
Wei Seng Foong said: Customer wants to confirm whether they can use higher voltage for EN pin than Vin.
Example. Vin=3.0V and EN=5.0V
Yes, unless it's less than the absolute maximum ratings.
Wei Seng…
Hi Oba,
Any particular reason why the customer wants to use this part? It is an old device using a voltage mode control system and has much lower performance than our newer parts.
TPS628513, TPS62826, TPS628303 or TPS628503 are much better alternatives…
Part Number: TPSM82822A Other Parts Discussed in Thread: TPS628303 Hi Team,
Does this device take Step Loads response really well?
I will hit this device with 1.2A step loads repeatedly, once every minute, and the output cannot dip.
Is this a good device…
Hello Mark,
Thank you for using E2E,
Since TPS54316 is very old part, I need to check internally for this rating and get back to you.
Please recommend the customers our latest devices such as TPS628303 data sheet, product information and support | TI.…