Part Number: TPS62840 I saw a previous support ticket ( https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1080447/tps62840-more-output-capacitance-than-recommended-cout_max-in-datasheet?tisearch=e2e-sitesearch&keymatch…
Part Number: TPS62840 HI, dear.
My intention is using TPS62842DGRR to produce 3.2V. When plug the type-c, the board is powered automatically and charge the battery meanwhile.
There is a strange problem. Actually when plug the type-c, the output of…
Part Number: TPS62840-1YBGEVM56 Other Parts Discussed in Thread: TPS62840 , Hi,
C12 given as X5R 0402, is it fine to use for temperature range -40 to 85 degree cel device ambient temperarure. is it reliable?
or shall we move to 0603 X7R.
and what…
Part Number: TPS62840 Dear Sir/Madam,
Thank you for your response.
For TPS61230DRC, We are find to locate this part number on your website; please confirm whether you can provide the requested data.
For TPS62840DLCR, we were unable to find the…
Part Number: TPS62840 Hi Experts,
The TPS62840 datasheet shows high-side Rds(on) typical values versus temperature (Figure 6), as well as maximum values for Vin of 3.6 V and 5 V.
1. Could you please provide data on high-side Rds(on) maximum values…
Part Number: TPS62840 Tool/software: Hello,
Our current project implements the TPS62840DLCR buck converter as the main 2.8V power supply of the device. Here is the schematic (with main test point in yellow, which will be used below) :
My problem…
Part Number: TPS62840
Hello,
I have configured the DC/DC to output a voltage of 3.3V. Although most of the time, the input voltage will be two CR2032 batteries (6V), sometimes the user might use a single CR2032 battery (3V). Will the DC/DC work in…
Part Number: TPS62840 Hello,
My customer is currently using the TPS62840DLC(Connect MODE pin/STOP pin to LOW (GND)) and is considering switching to the TPS62840YBG.
Their system requires the TPS62840's current consumption to be managed below nA. If…