The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Hello Youhei MIYAOKA,
Thank you for reaching out,
Youhei Miyaoka said: Is this limit fixed value? If so, please teach me.
Or is this limit value the same as the ILIMF of the power switch between 0.8 and 1.2A?
You can consider ILIMF as the current limit…
Hello Andre Nudel,
andre albagli said: Basically I will use a 5v Vin and 3.3v for Vout and maximum load current of 130 mA
Thank you for sharing the operating conditions.
Do you have any other requirements such as low quiescent current, high efficiency,…
Dear Customer,
Thank you for using E2E,
The output voltage ripple depends upon the output capacitor your are using and also on the tolerance of inductor and capacitor. I would recommend to use WEBENCH Power Designer (ti.com) to estimate the peak to peak…
Hello CSC,
The 400mA maximum current defined in the datasheet is the sum of ILOAD and IOUT. So the maximum IOUT for TPS62742 is 300mA.
I assume you are using only the IOUT for output. In this case your load is exceeding the maximum load conditions. …
Hello Peter,
Thank you for reaching out,
Peter Xu said: My customer wants to check if we have any solution that can output 0.6/0.65/0.9/1.3V with TLV627432?
The minimum output for TLV627432 is 1.2V, but we have other devices which can output your reequipments…
Part Number: TLV62568A Other Parts Discussed in Thread: TPS62088 , TPS62843 I couldn't find a specification in the component's datasheet specifying the output voltage tolerance/accuracy of the converter. The only mention of "accuracy" relevant to the converter…