Part Number: TPS628513 Tool/software: Hello! The datasheet verbiage makes it sound like SS/TR voltage will equal the output voltage.
Could you please confirm? We hope to PWM (with RC filter) into the SS/TR pin, with our PWM voltage at 1.8V. Our ideal…
Part Number: TPS628513 Tool/software: To whom it may concern I would like to know if there are any other types of analyses that may be done using PSPICE for TI apart from the transient anlyses, for which the circuits
are normally set up. Otherwise,…
Part Number: TPS628513 Tool/software: To whom it may concern I installed the latest version available from the TI website onto my computer. Seemingly that went flawless. Subsequently the PSPICE-TI library files for the TPS628513 device were downloaded…
Part Number: TPS628513 Other Parts Discussed in Thread: TPS628503 Hi
Could you please tell me about performance difference between TPS628513 and TPS628503?
Is there a performance difference between TPS628513 and TPS628503?
For example, if the same…
Part Number: TLV62585 Other Parts Discussed in Thread: TPS628513 , TPS628503 Tool/software: HI ,
Below is our schematics
The VOUT will be 3.8V and C320 we will keep NM.
We have to fine tune the RC circuit on the EN pin to adjust the power…
Part Number: TPS54318 Other Parts Discussed in Thread: TPS628503 , TPS628303 , TPS628513 Tool/software: Dear TI Forum,
I've measured the output voltage ripple of the TPS54318. Besides the switching noise of around 8mV_pp there is a beat frequency…
Part Number: TPS62088 Other Parts Discussed in Thread: TPS628513 As per datasheet, recommended is 2x10uF or one 22uF
let's assume for 3.3V output voltage. Customer is currently using 2x10uF . What if 5cm away there is an IC, that "requires" 100uf of…
Part Number: LM20125 Other Parts Discussed in Thread: TPS62816-Q1 , TPS62A06 , TPS628304 , LMZ10505 , TPS628513 , TPS54610 ,
Tool/software:
I have downloaded the TI transient reference design from TI & simulated in TINA but PGOOD is permanently low…
Part Number: TPS54317 Other Parts Discussed in Thread: TPS628503 , TPS628303 , TPS628513 Tool/software: Hi,
We use the TPS54317RHFR in our mass prodcut but we get the EOL file from TI,
So please kindly provide the new a lternative that we can evaluate…
Part Number: TPS62868 Other Parts Discussed in Thread: TPS628513 Hi Sir,
we want to adjust the Ramp speed, but seems that there is no response, ts there any special timing for this function?
may we know why can not be adjusted?
our setting sequence…