Part Number: TPS62864 Hi Team,
Customer is now evaluating a buck device with following technical requirements:
VOUT=2V-5V I2C adjustable
Iout≥4A
2 channels output is preferred, if it has one output also ok.
I checked TPS62864 which has the…
Part Number: TPS62864 Hello,
On part number TPS628640AYCG, the datasheet does not say what the voltage output range is on this part. You website states it, but the datasheet only says the turn on voltage is 0.4V to 1.15V. I want to use this part, but…
Part Number: TPS62864 Hi team,
My customer concerns about the pin spaing of WCSP package of TPS62864. My customer would like to meet telcordia standard by this device, and there are pin spacing limitation in telcordia standard. Is WCSP package of TPS62864…
Part Number: TPS62864 Tool/software: Hi team,
An external resistor must be connected at VSET pin of TPS62864.
When using TPS628640A, VID is available at A2 pin. Does it need resistor connected when VID is not needed?
When using TPS628640B, /PG is…
Part Number: TPS62864 Tool/software: Hello Team,
Can you please clarify what Iq exactly indicates? What is the occasion that the device is enabled by EN = high but not switching?
Eventually, I'm wondering how much of current is consumed in stand…
Part Number: TPS62864 Other Parts Discussed in Thread: TPS62868 , TPS62865 Hi team,
The customers are evaluating our TPS62864. Here are questions from customers.
1. why we have 2 registers in tps62864 with same VALUE (HEX) and OUTPUT VOLTAGE? how…
Part Number: TPS62864 Hi team,
I was hoping to get a cross for the KTB8399XEDAA-TR [WLCSP-15] ( datasheet here ). The specific PN is the bottommost PN in the below screenshot. I didn't see anything pop up on the cross reference tool and the TPS6286x…
Part Number: TPS62864 Hello,
We have a test board with the below schematic where VDD is connected to a 286mOhm load (emulating our DUT load condition). We have a shunt to connect/disconnect this load. When disconnected, the output is regulated normally…
Part Number: TPS62864 Hi team,
My customer wants to use TPS62864 to get a 0.6V output by external VSET resistor. But they concerns about the resistor's accuracy and drift effect on the output voltage.
The datasheet shows we can accept the 23.7kohm…