Part Number: TPS62867 Other Parts Discussed in Thread: TPSM82816
We have a converter need for 3.3V -> 1V / 3.4A at 90C. The TPS62867 looked like a good option but there is an additional requirement that there is 500uF of ceramic capacitance on the output…
Part Number: TPS62867 Other Parts Discussed in Thread: TPS54617 , TPSM82866A Hello,
I'd like to know about the differences in performance between PWM and PSM (Power Save Mode) (PFM) of TPS62867. What's better and what's worse?
In addition,…
Part Number: TPS62867 Hi Sir,
we want to change the inductor from 0.22uH to the 0.47uH,
since the switch frequency is 2.4MHz, we calculate it around 0.22uH, and modify 0.47uH is very different, is there any risk?
condition as follows:
Vin : 3.3V
Vout…
Part Number: TPS62867 Hi sir,
What's the PCB trace width from VOS to vout(22uF) and the PCB trace length limitation ?
Can I route the PCB trace from VOS to C load far away from TPS62867 ?
Part Number: TPS62867 Hi team, I'd like to know if the output discharge function works when VIN(=EN) is 0V. Is it possible to use it under this condition? And, if you have any waveform that can help, could you please share me? Sincerely. Kengo.
Part Number: TPS62867 For our internal project we used TPS62867RQYR buck converter for 5V to 1.0V (Output current=4.0A). Please review the design, layout and inductor chosen and let me know the comments.
Inductor(L15) Part Number : IHLP1212BZERR22M11 …
Part Number: TPS62867 Hello Team,
all related designs to the TPS62867 converter mention typical inductor values of 220nH, but we would like to increase this value to 1uH to limit the inductor ripple for smaller loads.
The datasheet mentions that any other…
Part Number: TPS62867 Hi
The VIN falling slew rate of TPS62867 is lower than Vulvo, and there are special suggestions. Like the red frame. -10mV/us, converted to -10000V/s, the slope is very steep.
(1) Here MIN, -10mV/us, does it mean that the power…
Part Number: TPS62867 For our internal project we used buck TPS62867RQYR to convert 5V to 1.0V(Iout=4A) . Please review the design and let me know the comments.
Part Number: TPS62867 Other Parts Discussed in Thread: TPSM82866A , Hi Team, May I ask for help? Our customer have a concern about TPS62867RQYR as shown below: 1.) Our application requires the device to operate in high temperature environment ~120-125 degrees…