Part Number: TPS62870-Q1 I see that the datasheet for the TPS62870-Q1 states that "Register contents remain intact as long as the input voltage remains above 1.4 V."
I was planning on using this device to generate a 0.9V rail. Does the output voltage…
Part Number: TPS62870-Q1 Hi team,
I found a description in the datasheet about unused SCL/SDA for I2C disabled variant and it requires to pull them to GND.
In my case, I plan to use I2C enabled device, but want to leave I2C unused.
In this case…
Part Number: TPSM8287A12 Other Parts Discussed in Thread: TPS6287B25 , TPS62870 , Tool/software: dears,
Our power modules, such as TPSM8287AXX, always have 3 thermal pads as below picture shows:
I checked the datasheet and EVM user guide, there…
Part Number: TPS6287B10 Other Parts Discussed in Thread: TPS62867 , TPS62870 Tool/software: Please help me check TPS6287B10/TPS628691A remote sense circuit, Thanks!
Power from connector to base board.
Part Number: TPS62442 Other Parts Discussed in Thread: TPS62870 , TPS62867 Tool/software: Hi,
We are evaluating products for a core power supply for ASICs and require a dual-channel solution with the following specifications:
Channel 1: DC-DC 3…
Part Number: TPS62872-Q1 Other Parts Discussed in Thread: TPS62870-Q1 Hi TI expert,
How about TPS62872-Q1 and TPS62870-Q1 part status? What's date for their mass production?
Thanks!
Michael.
Part Number: TPS62868 Other Parts Discussed in Thread: TPS62870 Tool/software: Buck or PSPICE team,
We have a customer trying to use the PSPICE model in frequency simulation to extract the output impedance.
Questions from them:
Is there an app note…
Part Number: TPS62874-Q1 Other Parts Discussed in Thread: TPS62870 , TPS62869 , TPS62870-Q1 , Tool/software: In design phase of an ASIC validation test board and considering the TPS62874 for the core voltage regulator. Application is 3.3 VIN, 0.5-0.55…
Part Number: TPS62867 Other Parts Discussed in Thread: TPS62870 Team,
I am building a discrete power sequencing as shown below
Can you please provide the maximum value of the High-level input threshold voltage at EN ? I would like to analyze distribution…
Part Number: LM21215A Other Parts Discussed in Thread: TPSM82866A , TPS62870 , TPSM82866C Tool/software: Hello,
My customer was using the LM21215AMHE-1 under the following conditions.
- INPUT : 5V, OUTPUT : 0.9V, LOAD : 6A
They designed the circuit…